This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are trying to collect 1 GB of samples per channel from the ADC32RF45 using the TSW14J56EVM, but have been having trouble collecting more than 33 million samples. It was suggested by someone from TI that we instead use TSW14J57EVM. We purchased the board, but the FMC connectors don't seem to be the same size (see pictures below). Will TSW14J57EVM not work with ADC32RF45? Or do we just plug the ADC32RF45 in and leave pins of the TSW14J57EVM empty?
Hi Claire,
The Connector on TSW14J57 is FMC+ and connector on ADC32RF45 is FMC. FMC+ connector is backwards compatible with FMC connector. If you try to center the FMC connector on ADC32RF45 with FMC+ connector on TSW14J57 it should connect. Also both of the connectors are keyed so there is only one position where they will connect to each other.
Regards,
Neeraj