Part Number: AFE5851
Other Parts Discussed in Thread: CDCLVD1216, AFE5832LP, AFE5816
Hi,
We have a design with multiple AFE5851 devices. They receive the same sample clock of 20 MHz and they generate their on 10 MHz frame clock.
However we have observed that the frame clocks are not in phase. See the picture below (ignore the labels) which shows the frame clock of 4 different AFE5851.
Since I believe the frame clock is in tight relation with the actual sampling moment, two of the above ADCs sample 50 ns later, then the other two.
Is there any way to synchronize them to each other? I was trying to achieve this with centrally controlled PDN signal, but it was not successful. The biggest
problem is, that after power-up different AD converters are synchronous than previously, which add random 50 ns variance between these devices.
thank you for the help.
regards,
Peter