Hi,
Issue is that above a static gain value of some 10 dB, the output signal keep the same gain whatever the value I set in coarse gain register.
The signal is not saturated but the gain do not increase.
SPI configuration is :
00 00 00 01
00 04 00 10
00 02 00 00
00 05 00 00
00 07 04 08
00 00 00 04
00 99 00 08
00 9A 00 1D
In this case, If I set 0x9A register to 0x24 instead of 0x1D => No effect.
Is there any other bit to configure or limitation I've miss in datasheet ?
NB: I've try to set INTER_ENABLE bit, but no change.
thanks for your support.
Fabrice