Part Number: ADS7142
Hello,
I'm working with the ADS7142 device using a STM32 ARM M4 processor with I2C. I have configured the 'Manual Mode Dual Channel Sampling' exactly as in the
'TN4C1294 Interface to ADS7142 Software Library' documentation (SBAA288–July 2018), page 25, Figure 14. The I2C communication works well (I see on the
scope the messages and the quality of the signal) but the data returned by the channels is not correct. The received values are changing all the time but are too big
and the measured voltage should be closed to zero. I see on the scope that the device indeed returns the values that I read on the buffer. The processor and the device
are on a custom designed board and the hardware engineers are confirming that is no problem with the hardware. I have tried to configure also only a channel but
the result is the same.
Please advise how to debug this issue.
Thank you in advance,
Sorin.