Part Number: DAC80504
We are planning to use DAC80504 in our application. we would want to give reference of 5V to REF pin. Our VDD is +5V. Datasheet says Reference input range can be equal to VDD if REFDIV is enabled. If we enable REFDIV(i.e, REFDIV=1), and Gain = 1, VOUT can be in range of 0-Vref. Does that mean Vout is 0-5V ?
As per our understanding we can give 5V external reference , then we will set REFDIV=1, GAIN=1 to get Output voltage range 0 to 5V. Please confirm.
Awaiting for the quick response.