Part Number: TSW14J56EVM
Other Parts Discussed in Thread: ADS54J20
Hello,
I have purchased TSW14J56 evaluation board combined with ADS54J20 to test and use with a LiDAR system. So far, I have used the functions provided by with the HSDC software and the ADC GUI, and everything seems to work properly.
Now, I would need to move forward. And to do so, I need to modify the firmware provided with the board (TSW14J56RevD Respin Fw.qar). My question is:
1) Is it possible to modify/customize the firmware and recompile for use?
2) Is it possible to develop and apply some DSP algorithm with the captured data before transfer to the PC?
3) Is it possible to make multiple custom triggers to start and stop data capture and transfer?
4) Is it possible to develop some custom interface/port to communicate with standalone firmware?
It can be mentioned that I have already restored the firmware provided with TSW14J56EVM (TSW14J56RevD Respin Fw.qar) and have no idea about how to proceed with that source files as I am new to FPGA and so far I understand only the source files are provided not complete project. Thanks in advance.
Kind Regards,
Dipak Kumar