Part Number: TSW14J56EVM
Other Parts Discussed in Thread: ADC34J45EVM
Dear all;
Hi.
I'm using TSW14J56EVM with ADC34J45EVM.
I developed a code under LABVIEW to make some analyzes on captured data from TSW14J56EVM.
Using the manual and examples in the "Texas Instrument" folder I was able to proceed with no problem.
All of a sudden, the LABVIEW program stopped working and even the provided example returns error codes 62 and 66.
From "DLL error codes" file, it seems that there is a problem with the connection between LABVIEW and HSDC Pro GUI.
As suggested, I re-opened the program, restarted the system and even reinstalled HSDC program but still getting the error code.
I should mention that HSDC works fine and I can capture from the GUI.
any help is more than welcome.
Thanks.