Part Number: ADS1120
Hello,
my customer is currently working a project with ADS1120 (VQFN Package) and they also to plan to measure temperature using the thermal pad of the device. the engineer would like to know if the thermal pad is floating or if it's internally connected? can they connect the pad to the metal housing (it's not connected to any potential) of their equipment in order to measure its temperature?
Also the device is used to measure voltage on a plug contact socket; however the engineer saw a deviation of approx. 150uV between what was captured by the ADC and the same voltage measured using a voltmeter. now he wants to know if its appropriate to use this device for this kind of measurement and if there are any care abouts to take into consideration.
Best regards,
Stani