Part Number: ADS5272
Hi Team,
Need your help regarding ADS5272 output coding scheme. Is the "Straight Offset Binary" the same with Bipolar Offset Binary in the below document? The ADS5272 datasheet states that a differential input of –1V corresponds to the zero code of the ADC, and a differential input of +1V corresponds to its full-scale code, which is quite the same with the BOB scheme.
http://www.ti.com/lit/an/sbaa042a/sbaa042a.pdf
Thanks in advance.
Regards,
Jejomar