Part Number: TSC2007
When we use our TSC2007 to realize the screen control.
But we met the problem with interrupt pin no response when we touch the screen.
Below is their schematic.
The address of IIC is 0x49. The configuration process is to configure the power-down mode in the initialization, and then click the screen to trigger the interrupt, configure the ADC digit and read the X and Y values through the interrupt processing function. But now they could not realize the interrupt response about the screen tough.
IIC should have no problem in reading and writing. By configuring d3-d2 01: A/D converter on. PENIRQ disabled, the interrupt pin can be directly lowered to trigger the interrupt, but clicking on the screen does not.
So about the problem, could you please give us some comments?