Hi there,
I intend to run two ADS1262 in parallel. Both shall convert at 50 SPS with a common external clock (7.373 MHz sourced from an FPGA - yes not exactly 7.3728 MHz). To allow other other measurements to run at the same sampling rate with a known phase shift I have implemented a counter that triggers all other measurements after 147'456 clock cycles (Table 8 in the datasheet: decimation ratos 8*64*288) to get exactly the same data rate.
Now the problem: Datasheet chapter 9.4.12
"As a result of the delay required by the digital filter to settle after reversing the inputs, the chop-mode data rate is less than the nominal data rate, depending on the digital filter order and programmed settling delay."
My setup works perfectly fine - as long as chop mode is disabled - which is NOT an option.
Is there anyone (probably TI insider) who can give me precise numbers (best in #fclk_cycles or us) how sinc1, sinc2, sinc3 and sinc4 affect the data rate? So I could correct my counter in the FPGA design.
Thanks and best regards
Simon