Other Parts Discussed in Thread: ADS1299, ADS1298
Hello,
I am facing here the same problem when recording ECG with the ADS1299-6
I used channel IN1P, IN1N, and BIAS_DRV to measure ECG using ADS1299. I had set SRB1 on and SRB2 to OFF, and included only channel 1 for bias generation with PGA gain = 2, But there were large amplitude of 50Hz noises and its harmonics (like 150Hz, 250Hz, etc), which was so large that it was impossible to observe the ECG signal. how can i reject the noise generated?
Any suggestions? Thanks in advance.