Part Number: ADS7885
Hi Team,
Need your help on this. We need to more information about the clock frequency and sampling rate response of the ADS7885. Our customer would like to know the sampling rate of the ADS7885 when operated at SCLK=30MHz.
We would like to use Figures 25 and 26 of the datasheet about this relationship. However, the 5V and 3V response on Figure 26 was given at SCLK=48MHz and 40MHz respectively. Is this the case? Or we can still use these tables to find the value of the sampling rate with respect to a defined supply current and frequency?
Thanks in advance.
Regards,
Jejomar