Other Parts Discussed in Thread: ADS112U04, ADS122U04EVM, ADS122U04
My setup:
I cant see the registers of the ADC, all jumpers are in the default configuration.
When I start the GUI first and connect the EVAL-board afterwards, then the GUI will not recognise the board.
When I conect the board first and start then the GUI software, I receive the message "Unable to Identify device = ADS112U04" and after a few seconds: " Hardware Connected. Ready..."
But I dont see any registers, even if I click Refresh.
Windows 7 64-Bit System
Installed software: - deltasigmaevalgui
- ads112u04evm-dvcpkg
In the device manager I see the following USB-Driver: Tiva Ware Bulk Devices - Generic Bulk Device
I installed the software on two different Win 10 PC, with and without Admin rights when I run the setup.
This solution doesnt help for my problem: 
Picture from device manager:
GUI: