Part Number: ADS1271
Other Parts Discussed in Thread: ADS1274, ADS1205, ADS1281
Hello. I am seeing some unexpected behavior when I use the ADS1271B and I could use some insight.
I am getting a radiated tone at 1/4096 of the modulator clock when I use the ADS1271B in modulator mode. I can switch to frame sync mode and the tone will go away. I have observed this behavior on the ADS1271EVM board as well as a custom board. It is my thought that the ADS1271B is using less chip resources when it is being used in modulator mode so I am puzzled as to why it is generating a tone. There are no tones on the input clock to the ADS1271B. The tone is not present anywhere else on the board when I use the ADS1271B in frame sync mode. I've used a spectrum analyzer and simply placed its probe on the ADS1271B body and the tone is quite visible. The tone is not radiating from any test equipment. Could someone lend some insight to this? If the modulator is used in both the modulator and frame sync modes why am I only seeing a tone in modulator mode?
Thank you for your time.