Other Parts Discussed in Thread: AMC1210, , ADS1203
Hi,
In one project, I need to transfer Analog signal from High voltage(Hot) side to Low voltage (Cold) side with at least 10kV isolation and at least 20kHz bandwidth(-3dB). I would like convert analog signal into digital signal first. The digital signal will be transferred to cold side with high isolation pulse transformer and then convert back to analog signal. The analog will be converter to current signal and transferred to remote location.
In this regard, I would like to use 1-bit stream AMC1203 or equivalent delta sigma modulators and AMC1210 or equivalent decimation filter to convert back to analog signal. Please let me know how AMC1203 can be interfaced with primary of pulse transformer and how secondary of pulse transformer interfaced with AMC1210. Thanks in advance.
Thanks and Regards,
Rajareddy