This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Specialists,
My customer is interested in ADS7043 and has a question.
I would be grateful if you could advise.
---
I'd like to use ADS7043 and AVDD=1.8V
The analog signal is interfaced by 1.8V and is directly received by ADS7043.
Could you please advise about Surge Protection circuit.
Generally, it uses TVS diode or Zener diode, but there is not 2V clamp diode.
What type of circuit should I use?
---
I appreciate your great help in advance.
Best regards,
Shinichi
Hello,
You are right, the most common protection is a diode.
What is driving the ADC input?
Is there a step down from a higher voltage power supply? Devices usually are limited to the highest voltage they are exposed to. If higher, how much higher is the power supply from 1.8V of the ADC input source?
Regards
Cynthia
Hi Cynthia,
Thank you for your reply.
In this case, ADC input is 0-1.8V directly from outside and power supply is 1.8V.
It only needs to be able to measure an approcimate value.
I couldn't find 1.8V zener diode.
I appreciate your great help.
Best regards,
Shinichi