Part Number: DAC7311
Hi Team,
DAC7311 is used for RF signal, but the output has high frequency harmonic which has bad effect on RF performance.
DAC7311 is powered by a 3.3V LDO and the output is set to 0.9V, the frequency spectrum of power supply is as below, it can be seen that the power supply is very clear at high frequency.
However, the output frequency spectrum shown below has high frequency harmonic at about 311kHz/631kHz/941kHz/1.251MHz. The output is disconnected with the load and is measured directly. The SPI clock frequency is 4.5MHz, that why there is 4.5MHz harmonic in the picture.
Could you please tell why the output has high frequency harmonic? Thanks!
Best Regards!
Hao