Part Number: ADCPRO
Other Parts Discussed in Thread: ADS1282
Hello,
I've been gathering some data using ADCpro and a ADS1282EVM board.
I also process data with matLab to ease comparing spectra. I think I'm finding some lack of coherence. The two spectra below are supposed to be from the same data :
To scale according to dBFS I just divided all data by « Max Code » included in the data text file generated by ADCPro.
I’ve tried a few different PSD (power spectral density) calculation techniques in MatLab and the dBFS noise floor is always at the same place, like 30dB lower than what is indicated by ADCPro.
Reading older posts related to this kind of problems I found :
and
The problem those users found could be the same I see.
In both cases there seems to be a possible bug in Y-scaling recognized from TI side, but in both cases the thread ends without a clear solution or work-around (as far as I can understand). Both are quite old.
Do you have updates on these topics ?
Would it be possible to have a detailed description on how dBFS values are calculated ?