Hi!
I have a problem when using adc12dj3200. after power up,pll is locked,and jesd link can be up in JMODE1 using default reg setting. but,if i re configure the reg to IJMODE0 ,pll is not locked,and jesd is not up.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
I have a problem when using adc12dj3200. after power up,pll is locked,and jesd link can be up in JMODE1 using default reg setting. but,if i re configure the reg to IJMODE0 ,pll is not locked,and jesd is not up.
Hi User,
To change the JMODEs you will first need to disable the JESD_EN by writing the value of 0x00 to register 0x200. Than you can write the value of 0x00 to register 0x201 to change to JMODE0 and than enable the JESD_EN by 0x01 to register 0x200.
Regards,
Neeraj