Part Number: DAC8571
Other Parts Discussed in Thread: ADS1115,
Hello,
We are thinking of improving the drive resolution of a system that it used in photographic focus stacking at micron levels, these are current and voltage mode drivers for driving Voice Coil and Piezoelectric Motors. Our system is now based around the MCP4725 12 Bit DAC and ADS1115 16 Bit ADC and works quite well, but I believe the addition of the DAC8571 will improve upon this. The main controller utilized is a Raspberry Pi 3B and the controlling code is written in Python.
Could you point to a reference example of the Python code used to control the DAC8571. We've purchased a couple DAC8571 already, but could use a couple samples in case I smoke these.
BTW the ADS1115 are absolutely beautiful parts to work with, I appreciate the effort in the design of the ADS1115 as I'm a semi-retired analog/RFIC designer and did quite a bit of precision analog chip design (have a couple patents on LDO and precision voltage dividers).
Best,
Mike
mawyatt2002@earthlink.net