Other Parts Discussed in Thread: ADS124S08
Hi Experts:
My customer is using the ADS114S08 with TC for the temperature measurement , the schematic is below , ( The /DRDY is floated)
When they change the setting with 03h register(00h to 0A,0B...) , the output is almost the same without change ( the input is 50mV, the output is 50mV as well),
The output is the same as the input even they adjust the input from 40mV ~80mV . Additionally, they the value they read from the register is the same as their setting.
The input offset is 1.2V ,and they used the internal reference which is 2.5V.
Please help to check the issue why the PGA setting doesn't take effect in this project.