Part Number: ADS1298
My ADS1298 board worked well seeing from the software and all the power-test point values were correct. However, when I power the MMB0 board today, the blue light segments show '8.', which is abnormal. And the software tells that 'download failed...reset the hardware'. TP7, TP10 and TP6 are incorrect: TP7=+7V (should be +5V), TP10=+3.3V (should be +1V), and TP6=+0.4V(should be -2.5V). I think it is the power supply issue. Could you please tell me what is going on here and how to fix it? Many thanks!