Part Number: ADS1232
Tool/software: WEBENCH® Design Tools
We are currently working with a dual channel adc ADS1232 in doing so we faced a problem. We connected three of these adcs (adc1, adc2, adc3) with the MCU in which each has it own dedicated DOUT, PWDN and Serial CLK pins connected to MCU. The SPEED, GAIN0, GAIN1, A0 are connected commonly with the MCU And XTAL 2 not connected to GND. When reading adc1 individually with a single load cell adc1 outputs proper voltage from the load cell but the other adcs outputs junk values. I have checked the adc1 data from both channels they are reading fine but the other adc2 & adc 3 are reading junk values. Does this mean that the adc damaged or the has faulty input?