Part Number: DAC39J84
Hi all,
I am trying to send data to DAC39J84 from Ultrascale+ JESD block.
My design works fine with the evaluation board (http://www.ti.com/tool/DAC37J84EVM)
However, on the custom build board the SYNC signal from the DAC is not performing as expected.
My JESD design: subclass1, 8 lanes, F = 1, K = 20, Line rate = 6.25 GBPS, Reference clock = 156.25, Sysref = 4.88 (sysref is same for DAC & FPGA), DAC clk = 625 Mhz.
Again, the design works fine on the eval board and the layout of the custom board is very similar. I checked clocks and spi configuration of the DAC and clock distributor (LTC6951) they operate as expected and voltage levels are ok.
Clocks:
OUT1 -> DAC clk = 625MHz
OUT2 -> DAC SYSREF = 4.88Mhz
OUT3 -> FPGA Refclk = 156.25Mhz
OUT4 -> FPGA SYSREF = 4.88Mhz
This is what is happening on the eval board (top -> SYNC; bottom -> sysref):
On the custom board SYNC is always high and I am not sure what can cause that. Apparently, its a popular problem:
https://e2e.ti.com/support/data-converters/f/73/p/574027/2131081?tisearch=e2e-sitesearch&keymatch=DAC39J84#pi320995=4
https://forums.xilinx.com/t5/Networking-and-Connectivity/JESD-RX-sync-not-asserted/td-p/892775
This is the flow:
1) Program clock distributor and align outputs (it supplies dac clk and FPGA clk; both SYSREF clocks are muted)
2) program FPGA
3) program DAC (here SYNC goes high and will never change)
4) supply SYSREF for ~ 1 sec (here SYNC pin should start toggling)
5) NOTE: JESD IP core can see the sysref as it assers tx_tready pin
Also, what does SYNC need to toggle? is it looking for SYSREF edge or K28.5 symbols?
Any ideas?