Part Number: DAC38RF85
Hello.
I need generate signal with 600 MHz bandwidth, in the 1.2GHz carrier friquency.
If I understand correctly, i need genegate quadrature signal in zero carrier frequency, with sample frequency 600MHz. In the DUC, need set NC0 frequency to 1200MHz.
SERDES rate, for this purpose - 1.25*(2/8)*600*16 = 3000MHz. Thith interpolation 12 DAC clk - 7200MHz.
But, FIR filers passband BW is 0.4 x Finput. And I don’t understand how to get a signal with a required bandwidth.