Part Number: TSC2003
Hi team,
Is it necessary to prepare external reference for TSC2003?
i.e. Can TSC2003 use touch-panel by internal reference?
Best regards,
Shota Mago
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TSC2003
Hi team,
Is it necessary to prepare external reference for TSC2003?
i.e. Can TSC2003 use touch-panel by internal reference?
Best regards,
Shota Mago
Hello Shota,
The internal 2.5V reference is only used for Vbat, AUX, or temperature measurements. The Touch panel measurements are taken using ratiometric conversions. Looking at the internal diagram, you can see that the ADC REF is taken directly from VDD. This also means that no external VREF is needed.
Regards,
Aaron