Part Number: ADS8684
Other Parts Discussed in Thread: ADS8688
Hi,
I'm currently trying to communicate with one ADS8684 on a Linux platform. I have build the ADS8688 driver and loaded my target.
Seems the communication is working well (at least when I check SPI signals with a logic analyzer, I have request and response in the frames).
I'm testing the ADS8684 with command line, there are offset, scale and raw data for each input.
Default offset is -32768 (why not!), scale is a strange value (why not!) but raw is always 65535, no matter the input voltage is. I'm not sure it's normal ?
=> I'm looking for a C sample code application I can build and run on Linux to communicate with the ADS8684 and basically read inputs voltage. Is there anything available I can use ?
Thanks for the help,
Regards,
Joel