Hello all,
I am following the calibration procedure for the Zero-Offset calibration (I set the multiplexer to midvoltage supply, so that both AINp and AINn are shorted to that voltage level. Their difference should be zero; I measure that a few times and average the output. The result is the offset, which I will remove from each subsequent reading).
The procedure seems to be working correctly, and the offset values are in the range defined by the specifications. However I tried 6 different boards and only see positive offset values. I am a bit puzzled by these results: shouldn't I see small values around 0, i.e. both positive and negative? Is anything strange in my setup?
Thanks in advance,
Luca