Part Number: ADS8363
If I follow the Minimum Configuration Example (chapter 9.1.2 on page 44), there are 2 formulas for Ffilter and R
With a tacq of 100 ns and a capacitor of 1nF as mentioned, I end up with R = 4.243 ohm and Ffilter = 221 MHz. This value looks strange to me…
Am I right saying that
- R should be less than 12 ohm to respect the input impedance (page 20)
- Ffilter should be 500 kHz to respect the anti-alias filter of the Nyquist theory when the sample rate is 1 MSPS
- C should be higher than 1nF (recommendation on page 44)
All those constraints don’t seem to fit with these 2 formulas.
Where is my misunderstanding ?
Regards
Mihir