Part Number: ADS1605
Hi team,
Customer found that the Δ-Σ ADC had the highest sampling frequency of 5M and its bandwidth (BW) was 2.45M (ADS1605). For isolated Δ-Σ ADC, the sampling frequency can be as high as 20MSPS, but the bandwidth is only 800K. (AMC1304x-Q1)
Customer has the following questions. Could you give some suggestions?
Why can the sampling frequency of isolated ADC be so significantly increased? But the bandwidth is reduced?
Why are isolated ADCs based on Δ-Σ modulator and there are no isolated ADCs in other architectures such as SAR?
Best Regards,
Amy Luo