I found that the normal Δ-Σ ADC has a sampling frequency of up to 5M and a bandwidth (BW) of 2.45M (ADS1605). For isolated Δ-Σ ADCs, the sampling frequency can be as high as 20MSPS, but the bandwidth is only 800K. (AMC1304x-Q1) Why is the sampling frequency of the isolated ADC so significant? But the bandwidth is reduced? Why are isolated ADCs based on delta-sigma modulators, and other structures (such as SAR or Pipeline) not?