Part Number: ADS7828
Hi
Questions as below
1)What is the function of the user option circuit?
2)Any ESD parts need in analog interface ? and the ESD parts will effect measurement result ?
3)Can the analog input measure the power supply directly? Need to add protection circuit to measure?
For example, when Vdd & Vref in are both 5V, can I directly measure the LDO output 5V voltage in CH0 ...etc