Part Number: ADS131A02
Other Parts Discussed in Thread: ADS131A04
Dear all
I would like to ask questions about clock source of ADS131A02.
1. According to Datasheet, the typical value of fCLKIN is 16.384MHz.
If a frequency larger than this value (for example, 20 MHz) is input, the conversion time is considered to be shortened.
Are there any other effects other than conversion time?
(Please let me know if there are any disadvantages when increasing the frequency.)
2.The data sheet shows that SPI SCLK can also be used as an external input clock. Furthermore, the frequency is in the same value range as fCLKIN. I think using SCLK is fine, but are there any disadvantages compared to using fCLKIN?
(If SCLK is used, if there are restrictions other than frequency, please let me know.)
Best Regards,
Y.Ottey