Part Number: ADS1299EEGFE-PDK
Other Parts Discussed in Thread: ADS1299
I have an ADS1299EEG FE Rev A board and I am trying to use it as an ECG front end.
I have three electrodes attached to a person with this placement.
They are connected to the ADS1299 through the J6 jumpers like so:
- LA -> CH1+
- RA -> CH2+
- LL -> CH3+
I collected data for 30 seconds, but the frequency was really high. While the average resting heart rate is 60 bpm or 1 Hz the signal I collected reported had a frequency of 60 Hz.
When I looked at the scope tab I saw that the signal did in fact have a very high frequency and the peaks were ~30 samples apart.
I'm not familiar with this hardware so I'm unsure if this is a mistake or if I should be performing some kind of post processing on the data.
Any suggestions on why I am getting such and odd recording?