Part Number: ADC3244
Hi, I have 5 ADC3244s in my system. They all get synchronize sample clocks and are operated in 2-wire mode. The problem is the Frame Clock is 2 samples wide for the data output and since they are set up individually, they don't all start converting at the same time. This leads to some with frame clocks 180 degrees out of phase with the others. What is the best way to accommodate this? Can I disable the input clocks while each chip is set up then start the the input clocks simultaneously? I'm not using the internal divider, but could SYSREF help in this instance?
Thanks,
Ryan