This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J69: ADS54J69

Part Number: ADS54J69


I am designing an ADC based board in which I have used ads54j69 ADC.

Most of the circuitry I copied from the evaluation board.

since I am designing the board to qualify for mil grade, for which temperature requirement is min -40 to max +85 deg.

the transformer considered in eval board is from the mini circuit and it works from -20 to +85 deg, which is not acceptable.

can you please recommend a transformer which can satisfy my application without changing any component other thank only transformer.