This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5263: problems with synchronization

Part Number: ADS5263

Hello folks. I have a problems with synchronization ads5263. I have device with ADC ads5263 and FPGA Cyclone V. For synchronization i use frame clock (ADCLK). At 100 MHz input ADC clock (clkp/clkn), device not sinhronize at temperature -5 celcius degrees. But if i reduce input ADC clock (clkp/clkn) to 98 MHz device is sinhronize.
What can it be?

Best regards, Val.