Hi, Dear Supports: I have questions below.
Q1: For power down pin PDN (pin 50), does it actually have a internal 20K pulled down to Ground?
Q2: To set device power down by hardware, pull down PWN pin to Ground or pull up it to DVDD?
Q3: The datasheet says pin SEN is pulled up to IOVDD with 20K internally, is this incorrect, the correct is to DVDD?
Q4: For pins of PDN, RESET, SCLK, SDIN, SEN, SDOUT, SYNCB, their power supply is DVDD?
Q5: Pin PDN and SDOUT can also be as indications of Fast-Over-Range, the indication signals are internally latched or unlatched? Because, if they are unlatched, and I want to see by LEDs, I need external lathers.
Q6: For JESD204B data outputs (D[A,B][0:3][P,M}, total 8 pairs), they work in AC couple with a serial 0.1uF each line. In my circuit, the receiver is FPGA, in the PCB layout, these serial 0.1uF capacitors should be placed close to ADS54J60 side, or close to FPGA side, especially when ADS54J60 and the FPGA are in different boards (connected by connector)?
Q7: Also for JESD204B data outputs (D[A,B][0:3][P,M}, total 8 pairs), datasheet page 83 shows, 100 ohm termination per pair. Should place these 100 ohm before serial 0.1uF (on ADC chip side), or after serial 0.1uF (on FPGA side)?