Part Number: AFE4490
Hi guys, I am trying to read some registers from ATE4490 using NXP iMX RT1064 MCU. Please see the attached wave forms where you can see the clock in blue and MOSI signals in yellow. I am initially send this 4 byte to CONTROL0: uint8_t CONTROL0ReadBuffer[4]={0x00,0x00,0x00,0x0F}; right after I am sending other 4 bytes to read LED2VAL: buffer[4]={0x2A,0x00,0x00,0x00};
Could you please double check for me what am I missing my configuration. May SPI baudrate is around 100KHz; and I also verified that the reset pin( pin 20) and power down pi(pin 29) are pulled up high.