This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8860: Hi, I have a question about offset error calculation.

Part Number: ADS8860

Hi, i was studying about calculating offset error in ADC system with TI precision LAB.

I can understand the concept of using typical offset error when we calculate the total error.

However, I cannot understand the equation of total offset error using squre and root.

Could you explain in more detail why we use this equation when we calculate with typical value?

Thanks,

Yun

  • Hello Yun,

    This type of addition is referred to as RSS, or Root,Sum,Squared.  It is a statistical method commonly used when adding normally distributed numbers.  There is a lot of information that you can search on the web that goes into more detail on why this method is used.

    In the above TI Precision Labs example, we could have simply added all of the errors, but this would have give an unrealistically high estimation for the total error.  The typical number is 1 sigma, but this implies that 68% of all devices are better than the typical!  If you have several components adding to the overall error, it is unlikely all devices will be near the 1 sigma value, many will be much lower. 

    Regards,
    Keith Nicholas
    Precision ADC Applications 

  • Hello Keith,

    Thank you very much!

    Yun