Hi,
We'd like learn some details about ADS8688. For an over current protection mechanism, we're planning to integrate the ADS8688 as main ADC converter, it will measure AC signals for 50/60 Hz and we have to capture every period of the signal precisely. Sampling rate is relatively low, about 7.6 kSPS, for this sampling rate; we will use an external clock/trigger module.
We're carefully examined the datasheet, to be sure, we've a few questions :
- Is the SPI output behave like FIFO buffer? Can we read all sampled data after a cycle?
- Can we do the same job without an external clock? ( Automatic mode? )
- Is there any resolution difference if we use +/-10V or +/-5V as voltage reference?
- Is there a problem if AUX_IN pin is connected to GND?
Regards,
Gokhan