Part Number: ADS1248
Other Parts Discussed in Thread: ADS1298
hi @ all
I would like to use the ADS1248 for recording several RTDs and analogue
Voltages.
For getting familiar with handling the ADS1248 I built up a test setup.
unfortunately, the recorded data output code is not as I have expected.
The ADS1248 is put into operation under following condition:
AVDD = 3.3V
DVDD = 3.3V
I'm using directly connected AIN0 and AIN1 Inputs for Measuring the applied Voltage Level.
AIN0 = 500mV (stipulated via external circuit)
AIN1 = connected to Ground
As a reference the internal ref. 2,048V is being chosen.
Register settings:
address = Value
0x0 = 0x01 //set AIN0/AIN1
0x2 = 0x30 //onboard ref. selected
0x3 = 0x90 //PGA = 1, 2000 SPS
0x4-0x7 = 0x00 //no OFC applicable, transmitted byte-wise
0x7-0x9 = 0x400000 //FSC Gain = 1, transmitted byte-wise
0xB = 0xFF // no excitation current needed
Expected Data output:
Output Code = 223 * VRTD/VREF
Output Code = 223 * 0.5V/2.048V
Output Code = 0x 1f 40 00
Actual read back output Data =0x 00 00 00 f0
I know, by the use of offset and gain register the output data can be scaled, however the actual result is a significant deviation from expected value.
Could you please check my register settings, if chosen adjustments are sufficient for running a normal ADC conversation ??
Best
Patrick