Hi
Can u explain in detail about Signal conditioning loop ?
Why the ADC input ( ADCINP and ADCINN) should be buffered and driven differentially from the MUX output ( MUXOUTP and MUXOUTN) ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Can u explain in detail about Signal conditioning loop ?
Why the ADC input ( ADCINP and ADCINN) should be buffered and driven differentially from the MUX output ( MUXOUTP and MUXOUTN) ?
Hi Shreyas,
The MUXOUT/ADCIN pins allow you to design and connect your own signal conditioning circuit for filtering/level-shifting/amplifying/buffering the input signal(s) to the ADS1158. By connecting this circuit after the MUX, you can potentially use a single amplifier circuit for buffering all 16-input channels.
A signal conditioning circuit is not always needed; however, the two most common use cases for this circuit are 1) to buffer the input signals and 2) for converting single-ending input signals to a fully-differential signals.
NOTE: In Fixed-Channel mode, the ADS1158's "MUXSCH" register does not have values to select AINCOM as one of the MUX input pins. AINCOM is only used in Auto-Scan mode. Therefore, if you use the AINCOM input pin, you will probably always be using the ADS1158 in Auto-scan mode, OR alternatively, you could short AINCOM to AIN15 and then use Fixed-channel mode to measure single-ended inputs on pins AIN0 through AIN14.