This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300EVM-PDK: Hardware circuit problem

Part Number: AFE4300EVM-PDK
Other Parts Discussed in Thread: AFE4300
Hello,
I had two problems using AFE4300EVM-PDK.
Firstly, there seems no U4 and U5 on the board.
Secondly, when I use it to measure some resistance. For example, IOUT0 and IOUT1 are used as the current source, VESNS0 and VSENS1 are used as voltage measurement points. Then I used an oscilloscope to detect the signal waveform at both ends of the resistor and got the result that there is signal at one end of the current output and almost nothing at the other end. I want to ask if it is normal for the current source to do this?
Many thanks,
Haoger