This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4142EVM: Isolated power supply for EVM

Part Number: ADS4142EVM

Hello,

I am designing an isolated measurement circuit. Its structure is as follows.

So the ADC needs an isolated power supply, in the ADS4142EVM data sheet, page 9. Table 3 shows three power supply options.

Which one should I choose? For the 1 and 2 options, can I connect the isolated voltage 3.3V directly to the J16? If it is option 3, should I connect the isolated voltage 1.8V directly to JP13 and JP14? What about J16 and J9 and J11?