Part Number: ADS1220EVM
Other Parts Discussed in Thread: UNIFLASH, , MSP430F5528, ADCPRO
Hi, sorry for the delay. The problem isn´t the drivers, because I have 2 boards and the other work normaly.
I finaly replace the MCU for a new one and I having problems to flash the code that is in the board documetation. The file in the folder C:\Program Files (x86)\ADCPro\plugins\evm\ADS1220\fw is a .A43 file. I am using a Launchpad MSP-EXP430G2 as hardware tool for flashing and Uniflash.
When I load the archive ads1220evm.a43 the result is:
Is the ads1220evm.a43 a flasheable image? if I click the chekbox "binary" and write from the dirección 00C3FFh, which it's supose to be the base adress for program memory, the flash is performed, but the board doesn´t work, no comunication via USB, no SPI activity, no oscilation in the crystal.
any help?