Other Parts Discussed in Thread: OPA365
Hello,
We plan to use the ADS7947 at the IF output of a tuner (R820T2), we want to use it at maximum speed (2MSPS). i have two questions regarding the implementation:
-Is it absolutely required to use an op amp in our case? as of now the differencital output of the R820T2 goes directly to the differencial channel 0 of ADS7947, with one 5R termination resistor on each side and a 470pF capacitor between each side. As per datahseet the R820T IF output is 1.0V Peak to Peak nominal (2.0V P-P max) and has a differential impedance of 2kΩ//5pF .
-which voltage reference level is advised and is a dedicated voltage reference required? I wonder wether we could directly use our existing 1.2V or 2.5V rails (used by the FPGA). The REF and REF_GND decoupling has been done as per datasheet recomendations.
Thank you.