Part Number: TLC2558
Other Parts Discussed in Thread: TLV2548
Hi Team,
My customer considers to replace TLC2558 to TLV2548 for existing their application because of delivery issue.
I was asked the following questions about Configuration Register.
1)
TLV2548 doesn't have blue part bits (D10 and D7 of TLC2558).
Is it possible to replace?
My customer set D10=0 and D7=0 for current TLC2558 application.
2)
TLV2548 has D10 (green part: internal reference voltage select) which TLC2558 doesn't have.
Which should my customer select 0 or 1 for this bit?
My customer use 5V power supply.
3)
My customer set D8=0 (red part) for current TLC2558 application.
Is there any concern if he use D(8,7)=00 (Conversion clock=internal OSC) for TLV2548?
I believe he should D(8,7)=01 for TLV2548 to replace however would like to confirm just in case.
Best Regards,
Yaita