Other Parts Discussed in Thread: , OPA2350, THS4521
Hi,
Can anyone help me with an application circuit design for ADS1278?
I would just need the circuit diagram with the necessary components for synchronous data acquisition.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Nived,
The ADS1278EVM-PDK user's guide shows an example circuit. This design uses the REF5025 + OPA2350 for the reference circuit, and the THS4521 for the input driver.
You mention synchronous data acquisition; do you need more than 8 channels in your system? If not, each of the ADC's in the ADS1278 are always synchronized to each other.
Regards,
Keith Nicholas
Precision ADC Applications
Hello Keith,
Thank you for your quick response. Actually I want to obtain 16 channel synchronous data ie. would like to use two ADS1278 in the daisy chain. Could you let me know where can I find that circuit?
Hello Nived,
I am not aware of a reference design, but the details are outlined in the datasheet.
You can daisy chain two ADS1278's using SPI for a total of 16 channels. Please note that your maximum output data rate for each of the channels will be limited due to the maximum SCLK frequency equal to FCLK. For SPI, FCLKmax=27MHz.
Operating the data converter in high resolution mode will limit your max data rate to 52.734Ksps for each channel. Figure 81 in the datasheet shows the necessary connections. SYNC, SCLK and CLK will be shared by both devices, your host MCU will monitor the DRDY line and when it pulses, you can transfer all 16 channels in one SPI frame.
Regards,
Keith